Standard object types supported - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document number
LIT-12013203
Revision date
2020-05-21

The following is a list of the standard object types as defined by ASHRAE that are currently supported in the Color TEC. See the section of the supported object type for details.

  • Analog Output
  • Analog Value
  • Binary Input
  • Binary Output
  • Calendar
  • Device
  • File
  • Multistate Value
  • Notification Class
  • Schedule
  • Trend Log