Network security options - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21
Non-secure Device - is capable of operating without BACnet Network Security
Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)
  Multiple Application-Specific Keys:
  Supports encryption (NS-ED BIBB)
  Key Server (NS-KS BIBB)