Character sets supported - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ANSI X3.4 IBM®/ Microsoft® Double-Byte Character Set (DBCS) ISO 8859-1
ISO 10646 Universal Character Set-2 (UCS-2) ISO 10646 (UCS-4) Japanese Industrial Standard (JIS) X 0208
ISO 10646 (UTF-8)