BACnet Interoperability Building Blocks (BIBBs) (Annex K) - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

The following table lists all BIBBs that are supported. The table is divided into BIBBs required for the BACnet Advanced Application Controller (B-AAC) profile, followed by additional BIBBs that are supported but not required for the B-AAC profile.

Table 1. BACnet B-AAC BIBBs Support
BIBB Name (A = Initiates and B = Executes) Designation
Required for B-AAC Profile
Data Sharing - Read Property - B DS-RP-B
Data Sharing - Read Property Multiple - B DS-RPM-B
Data Sharing - Write Property - B DS-WP-B
Data Sharing - Write Property Multiple - B DS-WPM-B
Alarm and Event - Notification - Internal - B AE-N-I-B
Alarm and Event - ACK - B AE-ACK-B
Alarm and Event - Information - B AE-INFO-B
Scheduling - Internal - B SCHED-I-B
Device Management - Dynamic Device Binding - A DM-DDB-A
Device Management - Dynamic Device Binding - B DM-DDB-B
Device Management - Dynamic Object Binding - B DM-DOB-B
Device Management - Device Communication Control - B DM-DCC-B
Device Management - Time Synchronization - B DM-TS-B
Device Management - UTC Time Synchronization - B DM-UTC-B
Device Management - Reinitialize Device - B DM-RD-B
Not Required for B-AAC Profile
Data Sharing - Write Property - A DS-WP-A
Data Sharing - COV - B DS-COV-B
Data Sharing - COVP - B DS-COVP-B
Alarm and Event - Alarm Summary - B AE-ASUM-B
Alarm and Event - Enrollment Summary AE-ESUM-B
Scheduling - External - B SCHED-E-B
Trending - Viewing and Modifying Trends Internal - B T-VMT-I-B
Device Management - Restart - B DM-R-B
Device Management - List Manipulation - B DM-LM-B
Device Management - PrivateTransfer - B DM-PT-B
Executes ReadRange Executes ReadRange