Optional relay - Johnson Controls - LIT-1901180 - CSDSC - Current Switch - CSDSC Series VFD and Constant Volume Current Switch

CSDSC Series VFD and Constant Volume Current Switch Catalog Page

Brand
Johnson Controls
Product name
CSDSC Series VFD and Constant Volume Current Switch
Document type
Catalog Page
Document number
LIT-1901180
Revision date
2021-08-13
Language
English
Figure 1. Optional relay Optional relay
  • Depth, 0.84 in.; height, 0.72 in.; width, 2.06 in.
  • Add the relay to the CSDSC switch to feature start, stop, and status functionality without the need for an independent device.
  • The relay is removable for service.
  • The relay reduces time, space, and the number of installed components.