Introduction - Johnson Controls - LIT-12013942 - CEGPNL100x-0 - JC-TMR2400-x - SE-CEG1001-x - Network gateway - CEG1001 Connected Equipment Gateway

CEG Network and IT Guidance Technical Bulletin

Product
Document number
LIT-12013942
Revision date
2022-02-21
Product status
Active

This document contains important information about connecting a Connected Equipment Gateway (CEG) to your network. From an IT perspective, a system device, such as a CEG, is simply a node on the network. However, the CEG uses communication protocols, security methods, and other technologies that you must consider carefully.

Important: Engage appropriate network security professionals to ensure that the digital certificates are handled. The IT organization must approve configurations that expose networks to the Internet. Be sure to fully read and understand IT compliance documentation for your site. Use care when you perform actions on system components because restarts may be required that conflict with compliance requirements. For example, when you upgrade firmware or install new SSL certificates, the computer may be offline for a period of time.