DHCP - Johnson Controls - LIT-12013942 - CEGPNL100x-0 - JC-TMR2400-x - SE-CEG1001-x - Network gateway - CEG1001 Connected Equipment Gateway

CEG Network and IT Guidance Technical Bulletin

Product
Document number
LIT-12013942
Revision date
2022-02-21
Product status
Active

Dynamic Host Configuration Protocol (DHCP) is a network management protocol that a network administrator can use to supervise and distribute IP addresses from a central point. DHCP automatically sends a new IP address when a device is plugged into a different location on the network. The network administrator can use DHCP to assign dial-up users an IP address automatically when they connect to the network. Some DHCP servers can support fixed addresses for devices that need a static IP address.

The CEG uses DHCP to obtain its IP address and other network information. Each device that connects to the Ethernet network needs a unique IP address. If a DHCP server is not used on the network, enter the IP address manually for each device. Also enter a new IP address if the devices are moved to another subnet on the network. The CEG supports both dynamic and static IP address assignments.