Wiring communications to SA-Bus - Johnson Controls - LIT-12013860 - CE360 Critical Environment Display

CE360 Critical Environment Display Installation Guide

Product
Controls > Critical Environment Controls > CE360 Critical Environment Display
Document type
Installation Guide
Document number
LIT-12013860
Revision date
2023-11-08
Figure 1. SA-Bus wiring diagram
Table 1. SA-Bus wiring diagram
Number Component
1 DIP switch
2 24 VAC power terminals
3 CE-360 Critical Environment Display
4 Controller