Description - Johnson Controls - LIT-12013860 - CE360 Critical Environment Display

CE360 Critical Environment Display Installation Guide

Product
Controls > Critical Environment Controls > CE360 Critical Environment Display
Document type
Installation Guide
Document number
LIT-12013860
Revision date
2023-11-08

The CE360 Critical Environment Display provides local room status indication, alarming and setpoint adjustment to meet the needs of a critical environment such as a hospital isolation room, compounding pharmacy, or laboratory.

The high definition touchscreen display with patented 360° Safety Halo™ immediately alerts building staff to changes in room status with audible alarming, color-coded screen graphics and a 360˚ Safety Halo which enables room status verification down long hallways.

Up to five CE360 displays can sit on a single SA bus, which gives you access to the same points from multiple locations inside or outside the room. The intuitive user interface supports two rooms that show five points each or a single room that shows 10 points.

You can program the CE360 from the display object in the pre-engineered .caf files for pressure control or volumetric offset with pressure override. You can download these .caf files from the licensing portal for free. For more information refer to the CCM Quick Start Guide (LIT-12014059).

Figure 1. CE360 Critical Environment Display