Properties page - Johnson Controls - LIT-12013860 - CE360 Critical Environment Display

CE360 Critical Environment Display Installation Guide

Product
Controls > Critical Environment Controls > CE360 Critical Environment Display
Document type
Installation Guide
Document number
LIT-12013860
Revision date
2023-11-08

The following table details what type of points the CE360 expects for the properties page in the display object. The CE360 only uses the point order in each property page to determine what the point means and how to use it. For example, point 2 expects a multistate value (MV) point with three states. Point 5 expects an MV point with five states and point 7 expects an analog value (AV) with units in minutes. See Table 1 for more information. Point 6 and 7 in the properties page are optional. For example, the R1_PRO_Zone1 page contains 7 points. The R2_PRO_Zone2 page contains 5 points. The CLEAN-EN and CLEAN-DURATION points do not apply to Zone 2 and the display object does not include them. See Table 1 for more information.

Table 1. Points in the properties page
Order Read/write Type State and units Point name
1 Read-only MV

0= Positive

1= Negative

2= Positive and negative

ISOLATION-MODE-LIMIT
2 Read-only MV

0= Positive

1= Negative

2= Neutral

ISOLATION-MODE-S
3 Writable MV

0= Positive

1= Negative

2= Neutral

ISOLATION-MODE
4 Read-only MV

0= Occupied

1= Unoccupied

2= Bypass

3= Standby

OCCUPANCY-MODE-S
5 Writable MV

0= Occupied

1= Unoccupied

2= Bypass

3= Standby

4= Not set

OCCUPANCY-OVERRIDE
6 Writable Binary value (BV) False or true CLEAN-EN
7 Read-only AV Minutes CLEAN-DURATION
Note:
  • You can change the point name.
  • You can restrict points to read-only at CE360 level. You can add restrictions to make other points read only by selection of their respective boxes in the display object. You cannot edit points marked as read-only in the read/write column.