Overview of the display object - Johnson Controls - LIT-12013860 - CE360 Critical Environment Display

CE360 Critical Environment Display Installation Guide

Product
Controls > Critical Environment Controls > CE360 Critical Environment Display
Document type
Installation Guide
Document number
LIT-12013860
Revision date
2023-11-08

In the CCT, you can find the display object on the Display tab under Features. The display object can have multiple pages. Each page can have multiple points from the .caf file. For more information, refer to the CCT Installation Instructions (LIT-12011529).