Second generation CARBOCAP technology - Johnson Controls - LIT-12012119 - Temperature Transmitter - CD-WAx-00-2 Series Wall Mount and Temperature Transmitters

CD-WAx-00-2 Series Wall Mount CO2 and Temperature Transmitters Product Bulletin

Product
Sensors and Meters > Carbon Dioxide Devices > CD-WAx-00-2 Series Wall Mount and Temperature Transmitters
Document number
LIT-12012119
Revision date
2021-03-26

Johnson Controls is licensed to integrate the new, silicon based CARBOCAP CO2 sensor into HVAC or Building Automation Systems. This sensor has several advantages: high accuracy, excellent stability, negligible temperature dependence, and ease of installation.

The structure of the diffusion-aspirated, single-beam dual-wavelength sensor is remarkably simple. It consists of an Infrared (IR) source, a sample cell, a tunable interference filter, and an IR detector. The tunable interference filter enables measurements at two wavelengths. As a result, references are measured accurately without the typically broad tolerances inherent in dual-beam sensors.

Dust, water vapor, and most chemicals do not affect the measurement accuracy of the sensor. No special software compensation patches are required, and the device requires no maintenance.