Features - Johnson Controls - LIT-1921505 - C-5230 - Accessory - C-5230 Pneumatic Signal Limiter
C-5230 Pneumatic Signal Limiter Catalog Page
- Product
- Switches and Electrical > Pneumatic Switches > C-5230 Pneumatic Signal Limiter
- Document type
- Catalog Page
- Document number
- LIT-1921505
- Revision date
- 2021-02-19
- independently adjustable high/low limits
- integral hypodermic needle test points
- field chosen supply source
- low volume with fast response
- compatible with dual supply systems
- output equals low limit when input signal is below low limit
- output equals high limit when input signal is above high limit
- output equals input when input signal is between the set points
- output equals input when input signal is between the set points
- the C-5230-2 is shipped with its regulator mounted for low limit application— for high limit applications the regulator must be removed and installed in the high limit location