The C-5226 Pneumatic Signal Transmitter repeats pneumatic transmission signals or selects the higher or lower of two pneumatic signal levels directly from the output of a controller. The C-5226 may also be used as a high or low signal limiter or a differential switchover device.
Refer to C-5226 Pneumatic Signal Transmitter Product Bulletin (LIT-7171430) for important product information.
Figure 1. C-5226 Pneumatic Signal Transmitter