The C-2040 Averaging Cumulator is a low volume output device designed to operate a controlled device or receiver-controller by averaging the output signals of two, three, or four controllers or transmitters. The Cumulator produces an output signal equal to the average of the input signals.
Refer to C-2040 Averaging Cumulator Product Bulletin (LIT-7171410) for important product information.