Description - Johnson Controls - LIT-1921205 - C-2040 Averaging Cumulator

C-2040 Averaging Cumulator

Brand
Johnson Controls
Product name
C-2040 Averaging Cumulator
Document type
Catalog Page
Document number
LIT-1921205
Revision date
2020-11-11
Language
English

The C-2040 Averaging Cumulator is a low volume output device designed to operate a controlled device or receiver-controller by averaging the output signals of two, three, or four controllers or transmitters. The Cumulator produces an output signal equal to the average of the input signals.

Refer to C-2040 Averaging Cumulator Product Bulletin (LIT-7171410) for important product information.