Editing machine tags - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 4.0

Branch License Manager License Portal Help

Brand
Johnson Controls
Metasys
Product name
Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
4.0
Revision date
2022-05-20
Language
English

About this task

To edit the machine tag for a machine listed in the Machines tab, complete the following steps:

Procedure

  1. In the Actions column, click the edit icon. The Edit Machine Tag dialog box appears.
  2. Enter the machine tag in the Machine Tag text box.
    Note: When you change the machine tag in the License Portal, an online machine that runs the Software Manager shows the updated value after the Software Manager's main screen is refreshed or when the Software Manager is restarted. For offline machines, the machine tag updates in the Software Manager after the next offline activation.
  3. Click Save.
    Note: If the machine is connected to the Internet, you can update the machine tag through the Software Manager. Refer to Software Manager Help (LIT-12012389).