Licenses sub-tab - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 4.0

Branch License Manager License Portal Help

Brand
Johnson Controls
Metasys
Product name
Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
4.0
Revision date
2022-05-20
Language
English

The Licenses sub-tab displays under the My Branch tab and the Customers tab. The sub-tab displays a list of all the licenses for software products associated with the BLM's branch or the branch a Super BLM if accessed through the My Branch tab. The sub-tab displays a list of customer licenses if accessed through the Customers tab. The Licenses sub-tab also displays a search and filter function. Use the filter to find licenses by the following categories:

  • Activated
  • Available
  • Expired

The following table provides an overview of the table in the Licenses sub-tab.

Table 1. Licenses table overview
Column name Description
Product

Displays the name and the highest base product version of the software product associated with the license.

Product Code

Displays the product code of the software product. The product code corresponds to the product ID in AOMS. This column is empty for products without product codes that are not available for purchase in AOMS.

Project Name Displays the project name.
Feature

Displays the number of features mapped to a product as a link if there is more than one feature or the feature name and version if there is only one feature.

You can click the link displayed in the column to display the Feature Name, Feature Description, and Feature Version.

Purchase Order

Displays the purchase order number.

AOMS Order #

Displays the AOMS order number associated with the software product order.

Status

Displays the status of the license. For licenses with an activated status, you can view the Activation Date in its tool tip by hovering over the status.

Machine Tag

Displays the machine tag of the machine on which the software product was activated. A machine tag provides a descriptive label for your machine within the License Portal. It is blank for licenses that are not yet activated.

Note: If necessary, the machine tag is shortened to fit in the available space. You can see the full machine tag and the system ID in its tool tip by hovering over the machine tag.
Actions

Displays the Choose Action menu, which includes the following options:

Note: The available Choose Action menu actions depend on the status of the license.