The following information is new or revised:
- Unlike previous releases, in SWM 3.0, a publisher can add multiple, bundled features to a product. With the implementation of bundled features, customers can create backward compatible products and license multiple features with a single license key. Updated impact of bundled features in My Tech Licenses tab, Orders sub-tab and Viewing product details.
- Updated the Orders sub-tab information to include subscriptions.
- Updated the Requests tab information as past technician license requests also display.