Deactivating a License Offline - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 3.0

Branch License Manager License Portal Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
3.0
Revision date
2020-10-30

Offline license deactivation has three steps. The license is unavailable for reuse until all three steps are completed. The following table provides details on the steps for an offline deactivation.

Table 1. Offline deactivation Steps
Step Application Internet connection required Step result Step function Link
1 License Portal Yes Download the license deactivation file Initiates the offline deactivation Starting a new offline deactivation
2 Software Manager No

Apply the license deactivation file to generate a license release file

Continues the offline deactivation Continuing an offline deactivation in the Software Manager

Also refer to Software Manager Help (LIT-12012389).

3 License Portal Yes Upload the license release file Completes the offline deactivation Completing an offline deactivation in the License Portal