Downloading software - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 2.1

Branch License Manager License Portal Help

Brand
Johnson Controls
Metasys
Product name
Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
2.1
Revision date
2020-01-20
Language
English

About this task

You can use the Software tab to download a software item.

Procedure

  1. In the Actions column, click the download icon. The Download Software dialog box appears.
  2. Select the checkbox next to each file that you want to download as a zipped folder.
    Note: Select the topmost checkbox to select or deselect all files. You can click the name of the software package to view and select individual files or subfolders to download instead of the entire software package. This may or may not be slower than if you select and download the entire software package.
  3. Click Download to download the selected files, or Cancel to exit the Download Software dialog box.
    Note: If you have issues with the download speed, see the different sections in Troubleshooting for more information.