Licenses sub-tab - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 2.1

Branch License Manager License Portal Help

Brand
Johnson Controls
Metasys
Product name
Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
2.1
Revision date
2020-01-20
Language
English

The Licenses sub-tab displays under the My Branch tab and the Customers tab. The sub-tab displays a list of all the licenses for software products associated with the BLM's branch or the branch a Super BLM if accessed through the My Branch tab. The sub-tab displays a list of customer licences if accessed through the Customers tab. The Licenses sub-tab also displays a search and filter function. Use the filter to find licenses by the following categories:

  • Activated
  • Available
  • Expired

The following table provides an overview of the table in the Licenses sub-tab.

Table 1. Licenses table overview
Column name Description
Product

Displays the name and version of the software product associated with the license.

Product Code

Displays the product code of the software product. The product code corresponds to the product ID in AOMS. This column is empty for products without product codes that are not available for purchase in AOMS.

Feature

Displays the feature name and feature version of the software product.

Purchase Order

Displays the purchase order number.

AOMS Order #

Displays the AOMS order number associated with the software product order.

Status

Displays the status of the license. For licenses with an activated status, you can view the Activation Date in its tool tip by hovering over the status.

Machine Tag

Displays the machine tag of the machine on which the software product was activated. A machine tag provides a descriptive label for your machine within the License Portal. It is blank for licenses that are not yet activated.

Note: If necessary, the machine tag is shortened to fit in the available space. You can see the full machine tag and the system ID in its tool tip by hovering over the machine tag.
Location

When you click the icon in the Location column, the details for the location associated with the license appears. A location is available only if a license is transferred to the company.

Actions

Displays the Choose Action menu, which includes the following options:

Note: The available Choose Action menu actions depend on the status of the license.