Standard Object Types Supported - Johnson Controls - LIT-12012608 - SI-VRFCBN02-0S - SI-VRFCBN02-0SA - SI-VRFCBN02-0SC - SI-VRFCBN02-0SE - SI-VRFCBN02-0SI - SI-VRFCBN02-0SJ - SI-VRFCBN02-0SN - SI-VRFCBN02-0SS - Bulb controller - BACnet VRF Smart Gateway

BACnet VRF Smart Gateway Protocol Implementation Conformance Statement

Product
Network and Communications > Gateways and Routers > BACnet VRF Smart Gateway
Network and Communications > BACnet > BACnet VRF Smart Gateway
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012608
Revision date
01/01/2018

The following is a list of the standard object types as defined by ASHRAE that are currently supported in this product.

Indoor units: Device Object, Analog Input, Analog Output, Binary Input, Binary Output, Multistate Input, Multistate output.

Outdoor units: Device Object, Analog Input, Binary Input, Multistate Input.