Character Sets Supported - Johnson Controls - LIT-12012608 - SI-VRFCBN02-0S - SI-VRFCBN02-0SA - SI-VRFCBN02-0SC - SI-VRFCBN02-0SE - SI-VRFCBN02-0SI - SI-VRFCBN02-0SJ - SI-VRFCBN02-0SN - SI-VRFCBN02-0SS - Bulb controller - BACnet VRF Smart Gateway

BACnet VRF Smart Gateway Protocol Implementation Conformance Statement

Product
Network and Communications > Gateways and Routers > BACnet VRF Smart Gateway
Network and Communications > BACnet > BACnet VRF Smart Gateway
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012608
Revision date
01/01/2018

Indicating support for multiple character sets does not imply that they can all be supported simultaneously.

ISO 10646 (UTF-8) IBM®/ Microsoft® DBCS) ISO 8859-1
ISO 10646 UCS-2 (UCS-2) ISO 10646 (UCS-4) JIS X 0208