Product Description - Johnson Controls - LIT-12012608 - SI-VRFCBN02-0SJ - SI-VRFCBN02-0SN - SI-VRFCBN02-0SA - SI-VRFCBN02-0SC - SI-VRFCBN02-0SS - SI-VRFCBN02-0SE - SI-VRFCBN02-0S - SI-VRFCBN02-0SI - Bulb controller - BACnet VRF Smart Gateway

BACnet VRF Smart Gateway Protocol Implementation Conformance Statement

Product
Network and Communications > Gateways and Routers > BACnet VRF Smart Gateway
Network and Communications > BACnet > BACnet VRF Smart Gateway
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12012608
Revision date
01/01/2018

The Johnson Controls® VRF Smart Gateway enables the integration of the Hitachi VRF system with the building automation system (BAS). The VRF Smart Gateway performs this function by communicating between the native H-link communications network of the Hitachi VRF system and the open building standard BACnet®/IP network. The VRF Smart Gateway intelligently provides the VRF device and point data over the BACnet/IP network in a way that the BAS can easily discover. The VRF Smart Gateway therefore requires little or no post-integration configuration within the BAS.