Power Supply - Johnson Controls - Part No. 24-10050-57 - Gateway/Router - BACnet Router

BACnet Router Installation Instructions

Product
Network and Communications > BACnet > BACnet Router
Document number
Part No. 24-10050-57
Document revision
B
Revision date
2018-05-01

The BACnet Router requires a dedicated 24 VAC, 25 VA minimum power supply. Use a 24 VAC SELV transformer at the appropriate rating. The minimum input voltage for the BACnet Router to operate properly is 20 VAC. Maximum power consumption is 25 VA.