MS/TP Modular Jack - Johnson Controls - Part No. 24-10050-57 - Gateway/Router - BACnet Router

BACnet Router Installation Instructions

Product
Network and Communications > BACnet > BACnet Router
Document type
Installation Guide
Document number
Part No. 24-10050-57
Document revision
B
Revision date
2018-05-01

The 6-pin modular jack labeled MS/TP is a service port for MS/TP Bus applications.

Refer to the MS/TP Communications Bus for BCPro System Technical Bulletin (LIT-12011908) for additional information and guidelines on wiring devices on an MS/TP trunk.