Ethernet Port - Johnson Controls - Part No. 24-10050-57 - Gateway/Router

BACnet Router Installation Instructions

Brand
Johnson Controls
Document type
Installation Guide
Document number
Part No. 24-10050-57
Document revision
B
Revision date
2018-05-01
Language
English

The Ethernet connection (10 or 100 Mbps) is an 8-pin RJ-45 network port (Figure 1). Use the Ethernet port to connect to IP networks.