About this task
During startup, the BACnet Router automatically initiates an LED test to verify the operational status of the LEDs. Immediately after connecting supply power, the following LED lighting sequence occurs:
Procedure
- The POWER, BAT FAULT, 10 LINK, FAULT, RUN, and PEER COM LEDs turn On, indicating that the operating system (OS) is booting up. (After 2 seconds, the LEDs may change states depending on site-specific network activity.)
- The BAT FAULT, PEER COM, and FAULT LEDs shut Off. The RUN LED flashes to indicate that the BACnet Router software is loading.
- The LEDs display the status of the BACnet Router. When the RUN LED goes On Steady, statup is complete, and the BACnet Router is operational.