After applying 24 VAC power, the BACnet Router requires approximately 2 minutes to start up and become operational. See the LED Test Sequence at Startup section.
Startup is complete and the BACnet Router is operational when the (green) RUN LED is On steady and the (red) FAULT LED is Off (Figure 1).
Important: Wait for the BACnet Router to complete the startup sequence and the RUN LED to go On steady before initiating any other action on the BACnet Router.