DIN Rail Mount Application - Johnson Controls - Part No. 24-10050-57 - Gateway/Router

BACnet Router Installation Instructions

Brand
Johnson Controls
Document type
Installation Guide
Document number
Part No. 24-10050-57
Document revision
B
Revision date
2018-05-01
Language
English

About this task

To mount the BACnet Router on a DIN rail:

Procedure

  1. Securely mount a 20 cm (8 in.) or longer section of DIN rail horizontally and centered in the space.
  2. Ensure that the bottom two mounting clips are pulled outward and snapped firmly into the extended position (Figure 1).
    Figure 1. DIN Rail and Mounting Clip Features on the Back of a BACnet Router

  3. Hang the BACnet Router by the DIN rail hooks (Figure 1) on the top track of the DIN rail, and position the BACnet Router DIN rail channel snugly against the tracks of the DIN rail.
  4. Push the bottom mounting clips up to secure the BACnet Router on the DIN rail tracks.
    To remove the BACnet Router from the DIN rail, snap the bottom DIN clips to the outward extended position, and carefully lift the BACnet Router off the DIN rail.