Installation - Johnson Controls - Part No. 24-10050-57 - Gateway/Router - BACnet Router

BACnet Router Installation Instructions

Product
Network and Communications > BACnet > BACnet Router
Document number
Part No. 24-10050-57
Document revision
B
Revision date
2018-05-01

Follow these guidelines when installing the BACnet Router:

  • Transport the BACnet Router in the original container to minimize vibration and shock damage to the router.
  • Verify that all the parts shipped with the BACnet Router.
  • Do not drop the BACnet Router or subject it to physical shock.
  • Do not open the BACnet Router housing (except the data protection battery compartment). The BACnet Router has no user-serviceable parts inside.