Important: When you install the AS-CBLTSTAT, ensure that the connected 8-pin cable does not apply excessive strain on the AS-CBLTSTAT. Damage to the wires can occur.
Use the following table to make connections from the end device to the field controller. Cut and tie back any unused wires.
Figure 1. AS-CBLTSTAT Phone Jack
Figure 2. AS-CBLTSTAT