Applications - Johnson Controls - Part No. 24-10143-721 - Gateway/Router

AS-CBLTSTAT Cable Adapter Installation Instructions

Brand
Johnson Controls
Document type
Installation Guide
Document number
Part No. 24-10143-721
Document revision
-
Revision date
2017-12-01
Language
English

The AS-CBLTSTAT cable adapter is intended to provide a connection between 8-pin TE-6700 Series sensors (also known as Metastats) and newer field controllers that do not have an 8-pin sensor connection. The adapter is plugged onto the controller side of the cable, and then the exposed leads are hardwired to the AIs and COM ports (as noted in Table 1).