Description - Johnson Controls - LIT-1900821 - AFEFN - AFEDN - Louver - AL6 Airflow Measuring Stationary Louver - AL3 Airflow Measuring Stationary Louver

AL3 and AL6 Airflow Measuring Stationary Louvers Catalog Page

Product
Dampers > Louvers > AL6 Airflow Measuring Stationary Louver
Dampers > Louvers > AL3 Airflow Measuring Stationary Louver
Document number
LIT-1900821
Revision date
2021-03-09

Since 1905, Johnson Controls has developed and refined air control products by providing the highest quality control dampers that fit your application and size requirements. Now we are including airflow measuring louvers in our product offering:

  • AL3 airflow measuring louvers feature stationary aluminum blades with aluminum sensor blades in a 3 in. (7.5 cm) deep aluminum frame.
  • AL6 airflow measuring louvers feature stationary aluminum blades with aluminum sensor blades in a 6 in. (15 cm) deep aluminum frame.

Refer to the AL3 and AL6 Airflow Measuring Stationary Louvers Product Bulletin (LIT-12011834) for important product information.