For a list of available data points that you can map
into the Equipment Controller for AD-1272 devices, see Table 1. The table headings are as follows:
- BACnet object
- The ID of a mapped BACnet object.
- Name
- The name of the data point in the CCT.
- Description
- The description of the data point in the CCT.
- Input/Output
- Input/output. The type of data point in the CCT:
- In indicates input
- Out indicates output
- Access
- Access to the data point:
- R indicates read only
- W indicates write only
- R/W indicates read/write. Use the EasyCAF tool to add this data point to miscellaneous inputs if necessary.
- Value type
- The type of data.
- Update rate
- How often the data point checks for the value on the SA Bus.
- Measuring system
- The measuring system in the CCT:
- Imp indicates imperial measurements
- Met indicates metric measurements
- Both indicates both imperial and metrics measurements
- Engineering unit
- The engineering unit of the data point that depends on the measuring system.
Some data points are dependent on one another because a BACnet object can be mapped in the package more than one time to form a group of dependent points. The group is highlighted with the same background in the following table. You can only select either no point, or one point from the group.
| BACnet object | Name | Description | Input/Output | Access | Value type | Update rate | Measuring system | Engineering unit | Application | ||
|---|---|---|---|---|---|---|---|---|---|---|---|
| A | B | C | |||||||||
| AV1 | T | Temperature | In | R | Float | 6 s | Imp | °F | |||
| Met | °C | ||||||||||
| AV2 | AF | Airflow | In | R | Float | 2 s | Imp | ft3/s | ✓ | ||
| Met | l/s | ||||||||||
| AV2 | AF | Airflow | In | R | Float | 2 s | Imp | ft3/min | ✓ | ||
| Met | l/min | ||||||||||
| AV2 | AF | Airflow | In | R | Float | 2 s | Imp | ft3/h | ✓ | ||
| Met | m3/h | ||||||||||
| Application ID | Application name and units | Comment |
|---|---|---|
| A | Airflow [l/s, ft3/s] | Airflow in l/s or ft3/s units |
| B | Airflow [l/min, ft3/min] | Airflow in l/min or ft3/min units |
| C | Airflow [m3/h, ft3/h] | Airflow in m3/h or ft3/h units |