Related documentation - Johnson Controls - LIT-12014421 - AD-1272 - Airflow Measuring Station - AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System

AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System SA Bus Integration Application Note

Product
Sensors and Meters > Air Measuring Systems > AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System
Document type
Application Note
Document number
LIT-12014421
Revision date
17/05/2024

For additional information on Equipment Controllers, see the following table:

Table 1. Related documentation
For information about: Refer to:
Programming and Commissioning Metasys Equipment Controllers Controller Tool Help (LIT-12011147)
CCT and Equipment Controller Package Licensing Software Manager Help (LIT-12012389)
MS/TP Communication, SA Bus rules and specifications MS/TP Communications Bus Technical Bulletin (LIT-12011034)