GSAB integration setup - Johnson Controls - LIT-12014421 - AD-1272 - Airflow Measuring Station - AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System

AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System SA Bus Integration Application Note

Product
Sensors and Meters > Air Measuring Systems > AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System
Document number
LIT-12014421
Revision date
2024-05-17

About this task

To set up GSAB integration, use a portable PC with the CCT software tool installed and connected to the Equipment Controller, and complete the following steps:

Procedure

  1. Use the appropriate device profile in the CCT to add an SA Bus device. See Table 1.
  2. Select the points for the AD-1272 device. See Commissioning tips for more information.
  3. Set up the SA Bus device address.
    Table 1. SA Bus device profile in the CCT for the AD-1272
    SA Bus device name Description
    AD-1272 Thermal dispersion airflow probe