Output data points as application inputs - Johnson Controls - LIT-12014421 - AD-1272 - Airflow Measuring Station - AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System

AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System SA Bus Integration Application Note

Product
Sensors and Meters > Air Measuring Systems > AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System
Document number
LIT-12014421
Revision date
2024-05-17

You can add Read/Write output data points to Miscellaneous inputs with the EasyCAF tool. This duplicates output points on the input side in the CCT to use for the application. See the following figures.

Figure 1. Adding data points to Miscellaneous inputs in EasyCAF
Figure 2. Miscellaneous inputs in the CCT