Adding GSAB devices using the CCT - Johnson Controls - LIT-12014421 - AD-1272 - Airflow Measuring Station - AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System

AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System SA Bus Integration Application Note

Product
Sensors and Meters > Air Measuring Systems > AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System
Document number
LIT-12014421
Revision date
2024-05-17

When you use the CCT to add GSAB devices, the dialog window includes the following options:

  • Application selection. When applications are available, it is mandatory to select one of them. This provides all the data points that belong to the application.
  • Data points selection. Some points are dependencies of other points. If you select a point with dependency, you cannot select its dependent points. See Point mapping for more information.
  • Optional: Point name prefix modification.
Figure 1. Add Device dialog window in the CCT