Cable connections - Johnson Controls - LIT-12014421 - AD-1272 - Airflow Measuring Station - AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System

AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System SA Bus Integration Application Note

Product
Sensors and Meters > Air Measuring Systems > AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System
Document number
LIT-12014421
Revision date
2024-05-17

See the following figures for the connection between the Equipment Controller and the AD-1272 device on the SA Bus terminal block.

Figure 1. AD-1272 host monitor terminals
Figure 2. Connection to Equipment Controller SA Bus terminal block
Callout Description
A Connection to the previous device on the SA Bus
B SA Bus terminal block
C Cable shield connection
D Connection to the next device on the SA Bus
Figure 3. Connection between Equipment Controller and AD-1272 device on the SA Bus
Callout Description
A SA Bus terminal block
B AD-1272 device

For detailed information about how to install and wire the AD-1272 unit, refer to the AD-1272 Advanced Thermal Dispersion Probe Airflow Measuring System Installation Instructions (LIT No. 12012552).