Downloading software - Johnson Controls - Metasys - LIT-12012944 - Software Application - Software Licensing - 4.3

ABCS License Portal Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012944
Version
4.3
Revision date
2023-08-16

About this task

You can use the Software tab to download a software item.

Procedure

  1. In the Actions column, click the download icon. The Download Software dialog box displays a list of all published versions available for download.
  2. If the software you want to download has a newer version available, a dialog box appears with the different software versions from which you can select the version. Select the software version to download and click Next.
  3. Select the checkbox next to each file that you want to download as a zipped folder.
    Note: Select the topmost checkbox to select or deselect all files. You can click the name of the software package to view and select individual files or subfolders to download instead of the entire software package. This may or may not be slower than if you select and download the entire software package.
  4. Click Download to download the selected files, or Cancel to exit the Download Software dialog box.
    Note: If you have issues with the download speed, see the different sections in Troubleshooting for more information.