Viewing machine details - Johnson Controls - Metasys - LIT-12012944 - Software Application - Software Licensing - 4.3

ABCS License Portal Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012944
Version
4.3
Revision date
2023-08-16

About this task

To view the details for a machine, click the expand icon for its row in the Machines table. The following table provides an overview for the expanded information that displays for all software product licenses associated with the machine. A Choose Action menu is also available.
Table 1. Expanded machine details overview
Column name Description
Product

Displays the name and version of the software product.

Product Code

Displays the product code of the software product. The software product code corresponds to the product ID in AOMS. This column is empty for products without product codes that are not available for purchase in AOMS.

Feature

Displays the feature name and feature version of the software product.

Purchase Order

Displays the customer purchase order number.

AOMS Order #

Displays the AOMS order number associated with the software product order.

Status

Displays the current status of a license.

Location

When you click the icon in the Location column, the details for the location associated with the license appears. A location is available only if a license is transferred to the company.

Actions Displays the Choose Action menu, which includes the following options:

Note: The available Choose Action menu actions depend on the status of the license.