To edit the machine tag for a machine listed in the Machines tab, complete
the following steps:
Procedure
In the Actions column, click the edit icon. The
Edit Machine Tag dialog box appears.
Enter the machine tag in the Machine Tag text box.
Note: When you change the machine tag in the License Portal, an online machine
that runs the Software Manager shows the updated value after the Software
Manager's main screen is refreshed or when the Software Manager is
restarted. For offline machines, the machine tag updates in the Software
Manager after the next offline activation.
Click Save.
Note: If the
machine is connected to the Internet, you can update the machine tag through
the Software Manager. Refer to the Software Manager
Help (LIT-12012389).