Announcements - Johnson Controls - Metasys - LIT-12012944 - Software Application - Software Licensing - 4.3

ABCS License Portal Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012944
Version
4.3
Revision date
2023-08-16

The Home tab displays any system or product announcements in the language selected for the portal. You can click an announcement name to open the Announcement dialog box. You can view the announcement name, date, and announcement content, and you can click the announcement attachment to open the attachment if available. You can also search for an announcement. Announcements are used to communicate information such as portal downtimes and the availability of new product software versions.

If the announcement email contains marketing content, you can click Unsubscribe at the bottom of the announcement to unsubscribe. Option to unsubscribe is visible in the email announcement only. Alternatively, you can unsubscribe from Preferences page.Select the reason for unsubscribing and click Unsubscribe. You can select one of the following options:
  • Emails are too frequent
  • Emails are not relevant
  • I don't want to receive marketing emails
  • Other
The following message displays when you unsubscribe: You have successfully opted out of receiving marketing announcement emails. You can opt back in by accessing Preferences after logging in to your account.