The ABCS License Portal has different tabs available, see Table 1 . For some tabs, a Choose Action menu is available that has additional actions. The following table lists the actions available in the different Choose Action menus. Some actions are available in multiple tabs. The available actions can depend on if the license status is Available or Activated, if an offline deactivation is already in-progress for a license, or the user's role. See Glossary for more information.
Note: In some tabs, additional actions are available outside of the Choose
Action menu.
Tab | Available actions in the Choose Action menu |
---|---|
Orders |
|
Licenses |
|
Machines |
|
Users |
|