Verifying wireless operation - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

About this task

Note: When you first power up the wireless network, there is a potential for a few field controllers to toggle online and offline for a short period until the entire trunk has finished its startup procedure. This is a normal operation.
Note: Verify that all WEFCs have been discovered. To check the performance of the wireless mesh network, including online status and wireless signal strength, you can use the Diagnostics of the WRG1830.

To verify wireless operation follow one of the following methods:

Procedure

  1. Log into WRG1830 Gateway and view connected devices.
  2. Log on to the Supervisory Controller using the Launcher and view connected devices.