SSL settings - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Brand
Facility Explorer
Product name
WRG1830/ZFR183x Pro Series
Document type
Technical Bulletin
Document number
LIT-12013796
Revision date
2021-05-17
Language
English

If an SSL certificate is installed, the SSL settings screen, as shown in Figure 1 shows the currently installed security certificate and allows you to install both a Private Key and a new certificate. Only an Admin user can perform the following procedure. Refer to the Mobile Access Portal Gateway Network and IT Guidance Technical Bulletin (LIT-12012015) for information on how to use SSL Certificates in a WRG1830.

The WRG1830 uses security certificates to authenticate itself to web browsers. Refer to the Mobile Access Portal Gateway Network and IT Guidance Technical Bulletin (LIT-12012015) for more information.

Figure 1. WRG1830 Gateway SSL settings screen