Installing the WRZ Series Sensors - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

About this task

To install a WRZ Series Sensor, complete the following steps:

Procedure

  1. Select a mounting location for the sensor. Refer to the job site plans and the Occupancy Sensing WRZ Series Wireless Room Sensors Installation Instructions (Part No. 24-10332-96).
  2. Place the mesh application DIP switch overlay label over the DIP switches.
  3. Set the WRZ Sensor DIP switches as shown in Table 1.
    Table 1. WRZ Sensor DIP switch
    DIP Switch Setting
    Mode Mesh
    Zone Set according to application requirements.
    Transmit Level 10 mW
    MS/TP Address Match the MS/TP address of the associated device ( PCG/PCX/PCV16).
    PAN OFFSET Match the PAN OFFSET of associated ZFR Pro Coordinator and ZFR Pro Routers.
    Power OFF
  4. Verify that the factory calibration jumper is installed. If the jumper is missing, temperature readings report as unreliable values.
  5. Install two AA alkaline batteries supplied into the battery compartment on the back of the sensor. Ensure that you install the batteries in the correct polarity.
  6. Secure the sensor to its mounting base. Keep the power off until the wireless field bus system is ready to be commissioned.
    Important: The WRZ Sensor must have addressing switches set and then be powered up with the join network process of device discovery at the WRG Gateway.

    Repeat these steps for each additional zone sensor.