Installing the NSW Series Sensors - Facility Explorer - LIT-12013796 - Wireless Device - WRG1830/ZFR183x Pro Series

WRG1830/ZFR183x Pro Series Wireless Field Bus for Facility Explorer Systems Technical Bulletin

Product
Document number
LIT-12013796
Revision date
2025-02-07
Product status
Active

About this task

To install an NSW8000 Series Sensor, complete the following steps:

Procedure

  1. Select a mounting location for the sensor. Refer to the job site plans and the NSW8000 Series Wireless Network Sensors Installation Guide (LIT-12014419).
  2. Set the NSW8000 Sensor DIP switches as shown in the following table.
    Table 1. NSW Sensor DIP switch
    DIP switch Setting
    Mode Mesh
    Area Set to 0
    Zone Set according to application requirements
    MS/TP Address Match the MS/TP address of the associated device (FEC/IOM/VMA16)
    PAN OFFSET Match the PAN OFFSET of the associated ZFR Pro Coordinator and ZFR Pro Routers
    Power OFF
  3. Install two AA alkaline batteries (supplied) into the battery compartment on the back of the sensor. Ensure that you install the batteries in the correct polarity.
  4. Secure the sensor to its mounting base. Keep the power off until the wireless field bus system is ready to be commissioned.

    Repeat these steps for each additional zone sensor.